5.5 Default Connection
m2m_wifi_default_connect API. This API does not require AP
information to establish the connection. enum tenuCredStoreOption. The credentials such as passphrase of the AP or Enterprise certificate and
other parameters like SSID, IP address, BSSID are encrypted using AES128-CBC before they
are written into the serial Flash. This makes it difficult for an attacker to retrieve
the sensitive information even if an attacker has physical access to the device. If
there is no cached profile or if a connection cannot be established with any of the
cached profile, an event of type M2M_WIFI_RESP_DEFAULT_CONNECT is
delivered to the host driver indicating failure.
Upon successful default connection, the host application can read the
current Wi-Fi connection status by calling m2m_wifi_get_connection_info
API. The m2m_wifi_get_connection_info is an asynchronous API. The
actual connection information is provided in the asynchronous event
M2M_WIFI_RESP_CONN_INFO in Wi-Fi callback. The callback parameter
of type tstrM2MConnInfo provides information about AP SSID, RSSI (AP
received power level), security type, IP address obtained by DHCP.