6.3.3 UDP Client Operation
The following figure shows the flow for transferring data with a UDP client.

Note:
- The first send message must
be performed with the
sendtoAPI with the destination address specified. - If further messages are sent
to the same address, the
sendAPI can also be used. For more details, refer to send. recvcan be used instead ofrecvfrom.