1.15.2.25 CCPx_Compare16bitValueGet Function

C

/* x = CCP instance number */

uint16_t CCPx_Compare16bitValueGet( void )

Summary

Reads the timer current count value.

Description

This function reads the timer count value.

Precondition

CCPx_CompareInitialize() function must have been called first.

Parameters

None.

Returns

uint16_t - The timer's current count value.

Example

uint16_t counter = 0;
CCP1_CompareInitialize();
CCP1_CompareStart();
counter = CCP1_Compare16bitValueGet();

Remarks

The caller must know the number of significant bytes of timer. Period value is right-aligned.