1.15.2.28 CCPx_Compare16bitRAValueSet Function

C

/* x = CCP instance number */

void CCPx_Compare16bitRAValueSet( uint16_t compareValue )

Summary

Writes compare value of the given compare channel 0.

Description

Set CC[0] compare value.

Precondition

CCPx_CompareInitialize() function must have been called first.

Parameters

Param Description
compareValue value to set for compare channel 0

Returns

None.

Example

uint16_t compareValue = 0x100;
CCP1_CompareInitialize();
CCP1_Compare16bitRAValueSet(compareValue);

Remarks

None