1.2.15.13 PDECx_HALLPatternSet Function

C

bool PDECx_HALLPatternSet ( uint8_t pattern ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.

Summary

Writes the hall pattern.

Description

This function writes the hall pattern in CC0 LSB.

Precondition

PDECx_HALLInitialize function must have been called first for the given channel.

Parameters

Param Description
pattern hall pattern

Returns

true - If hall pattern set false - If hall pattern is not set

Example

uint8_t position;

PDEC_HALLInitialize();
PDEC_HALLStart();
PDEC_HALLPatternSet(0x3);

Remarks

None