1.2.15.14 PDECx_HALLTimeWindowSet Function
C
bool PDECx_HALLTimeWindowSet ( uint16_t low_window, uint16_t high_window ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Writes the low and high window threshold for hall mode
Description
This function configures low and high window threshold values.
Precondition
PDECx_HALLInitialize function must have been called first for the given channel.
Parameters
Param | Description |
---|---|
low_window | lower window threshold CC0[MSB] |
high_window | higher window threshold CC1[MSB] |
Returns
true - If Time Window set false - If Time Window is not set
Example
PDEC_HALLInitialize(); PDEC_HALLStart(); PDEC_HALLTimeWindowSet(1000, 60000);
Remarks
Window counter COUNT (MSB) is compared against low and high window threshold and if the counter is outside the window, error flag is set. This can be used to detect if motor is running too slow or too fast.