1.26.9.12 PIO_PinWrite Function
C
void PIO_PinWrite(PIO_PIN pin, bool value)
Summary
Writes the selected pin.
Description
This function writes/drives the "value" on the selected I/O line/pin.
Precondition
The desired pin must be configured as an output pin in MHC Pin Manager. PIO_Initialize() must have been called.
Parameters
Param | Description |
---|---|
pin | One of the IO pins from the enum PIO_PIN |
value | value to be written on the selected pin: |
- true | set pin to high (1). |
- false | clear pin to low (0). |
Returns
None.
Example
PIO_PinWrite(PIO_PIN_PB3, true);
Remarks
None.