1.26.9.6 PIO_PortClear Function

C

void PIO_PortClear(PIO_PORT port, uint32_t mask)

Summary

Clear the selected IO pins of a port.

Description

This function clears (to '0') the selected IO pins of a port.

Precondition

None.

Parameters

Param Description
port One of the IO ports from the enum PIO_PORT
mask A 32 bit value in which positions of 0s and 1s decide which IO pins of the selected port will be cleared.
  • 1's Will clear corresponding IO pins to low (to 0).

  • 0's Will remain unchanged.

Returns

None.

Example

// Clear PC5 and PC7 pins to 0
PIO_PortClear(PIO_PORT_C, 0x00A0);

Remarks

If the port has less than 32-bits, unimplemented pins will be ignored. Implemented pins are Right aligned in the 32-bit value.