1.26.9.14 PIO_PinLatchRead Function

C

bool PIO_PinLatchRead ( PIO_PIN pin )

Summary

Read the value driven on the selected pin.

Description

This function reads the data driven on the selected I/O line/pin. Whatever data is written/driven on I/O line by using any of the PIO PLIB APIs, will be read by this API.

Precondition

None.

Parameters

Param Description
pin One of the IO pins from the enum PIO_PIN

Returns

Returns the value driven on the selected I/O pin.

Example

bool value;
value = PIO_PinLatchRead(PIO_PIN_PB3);

Remarks

To read actual pin value, PIO_PinRead API should be used.