1.5.16.23 PDECx_COUNTERCompare1Get Function
C
uint16_t PDECx_COUNTERCompare1Get ( void ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Reads Compare 1 register value
Description
This function reads Compare 1 (CC1) register value.
Precondition
PDECx_COUNTERInitialize function must have been called first for the given channel.
Parameters
None.
Returns
Returns Compare 1 register value.
Example
uint16_t value; PDEC_COUNTERInitialize(); PDEC_COUNTERStart(); value = PDEC_COUNTERCompare1Get();
Remarks
None.