1.5.16.21 PDECx_COUNTERCompare1Set Function
C
bool PDECx_COUNTERCompare1Set ( uint16_t compare1 ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Configures Compare 1 register value
Description
This function configures Compare 1 (CC1) register value.
Precondition
PDECx_COUNTERInitialize function must have been called first for the given channel.
Parameters
Param | Description |
---|---|
compare1 | Value to be set in Compare 1 register |
Returns
true - If Compare 1 register set false - If Compare 1 register is not set
Example
PDEC_COUNTERInitialize();
PDEC_COUNTERStart();
PDEC_COUNTERCompare1Set(0x100);
Remarks
None.