1.41.6.8 HEMC_NoFixCallbackRegister Function
C
void HEMC_NoFixCallbackRegister(HEMC_CALLBACK callback, uintptr_t context)
Summary
Sets the pointer to the function (and it's context) to be called when the given HEMC's ECC Not Fixable Error interrupt events occur.
Description
This function sets the pointer to a client function to be called "back" when the given HEMC's interrupt events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called. The specified callback function will be called from the peripheral interrupt context.
Precondition
HEMC_Initialize must have been called for the associated HEMC instance.
Parameters
Param | Description |
---|---|
callback | A pointer to a function with a calling signature defined bythe HEMC_CALLBACK data type. Setting this to NULL disables the callback feature |
context | A value (usually a pointer) passed (unused) into thefunction identified by the callback parameter |
Returns
None.
Example
void APP_HEMC_NoFixHandler(uintptr_t context)
{
}
HEMC_NoFixCallbackRegister(&APP_HEMC_NoFixHandler, (uintptr_t)NULL);
Remarks
None.