1.32.18.22 PDECx_COUNTERCompare0Get Function
C
uint16_t PDECx_COUNTERCompare0Get ( void ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Reads Compare 0 register value
Description
This function reads Compare 0 (CC0) register value. This can be period value of the counter if CTRLA.PEREN bit is set.
Precondition
PDECx_COUNTERInitialize function must have been called first for the given channel.
Parameters
None.
Returns
Returns Compare 0 register value.
Example
uint16_t value; PDEC_COUNTERInitialize(); PDEC_COUNTERStart(); value = PDEC_COUNTERCompare0Get();
Remarks
None.