1.34.6.15 HSMCI_BlockCountSet Function

C

void HSMCI_BlockCountSet ( uint16_t numBlocks )

Summary

Sets the number of blocks to transfer

Description

Sets the number of blocks to transfer for a multi-block transfer. For example, the block count must be set to the appropriate value before issuing the multi-block read (CMD 18) or write (CMD 25) commands. For single blcok read (CMD 17) or write (CMD24) commands, the block count must be set to 1.

Precondition

HSMCI_Initialize() must have been called first.

Parameters

Param Description
numBlocks Number of blocks to transfer

Returns

None.

Example

HSMCI_BlockCountSet(1);

Remarks

None.