1.22.24.4 SDHCx_IsWriteProtected Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ bool SDHCx_IsWriteProtected ( void )
Summary
Returns the write protect switch pin level
Description
Returns the write protect switch pin level
Precondition
SDHCx_Initialize() must have been called first for the associated instance.
Parameters
None.
Returns
true - If the card is write protected.
false - If the card is write enabled.
Example
if (SDHC1_IsWriteProtected() == false) { // Card is not write protected }
Remarks
None.