1.12.14.9 MCPWM_Initialize Function

C

void MCPWM_Initialize (void)

Summary

Initializes given instance of MCPWM peripheral

Description

This function initializes given instance of MCPWM peripheral with the values configured in MCC GUI. This initializes all the selected generators of given peripheral in MCC GUI.

Precondition

MCC GUI should be configured with the right values.

Parameters

None.

Returns

None.

Example

MCPWM_Initialize();

Remarks

This function must be called before any other MCPWM function is called. This function should only be called once during system initialization.