1.12.14.6 MCPWM_PrimaryPeriodSet Function

C

void MCPWM_PrimaryPeriodSet (uint16_t period)

Summary

Sets the period value of the primary time base

Description

This function writes the period value of the primary time base generator.

Precondition

MCPWM_Initialize() function must have been called first for the associated instance.

Parameters

Param Description
period period value corresponding to MCPWM frequency

Returns

None.

Example

MCPWM_Initialize();
MCPWM_Start();
MCPWM_PrimaryPeriodSet(0x500);

Remarks

None