1.1.11.3 I2CSMBx_Read Function

C

/* x = I2C SMBUS peripheral instance number */

bool I2CSMBx_Read(uint16_t address, uint8_t* rdata, size_t rlength)

Summary

Reads data from the slave.

Description

This function reads the data from a slave on the bus. The function will attempt to read rlength number of bytes into rdata buffer from a slave whose address is specified as address. The I2C Master generates a Start condition, reads the data and then generates a Stop Condition. If the slave NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2CSMBx_ErrorGet() function to know the cause of the error. The function is non-blocking. It initiates bus activity and returns immediately. The transfer is completed in the peripheral interrupt. A transfer request cannot be placed when another transfer is in progress. Calling the read function when another function is already in progress will cause the function to return false. The library will call the registered callback function when the transfer has completed if callback is registered.

Precondition

I2CSMBx_Initialize must have been called for the associated I2C instance.

Parameters

Param Description
address 7-bit / 10-bit slave address.
rdata pointer to destination data buffer where the received data should be stored.
rlength Number of bytes to be read

Returns

true - The request was placed successfully and the bus activity was initiated

false - The request fails, if there was already a transfer in progress when this function was called

Example

uint8_t myData [NUM_BYTES];
void MyI2CCallback(uintptr_t context)
{
    // This function will be called when the transfer completes. Note
    // that this function executes in the context of the I2C interrupt.
}

I2CSMB0_CallbackRegister(MyI2CCallback, NULL);

if(!I2CSMB0_Read( SLAVE_ADDR, &myData[0], NUM_BYTES ))
{
    // error handling
}

Remarks

None