1.32.16.11 NVMCTRL_RegionLockStatusGet Function

C

uint32_t NVMCTRL_RegionLockStatusGet (void);

Summary

Returns the value of RUNLOCK register.

Description

This function can be used to know which of the regions are locked. Each bit in the RUNLOCK register corresponds to one region. Bit position zero represents the lock state for region starting at address 0x00000000.

Precondition

None.

Parameters

None.

Returns

Returns the value of RUNLOCK register.

Example

rlock_state = NVMCTRL_RegionLockStatusGet();

Remarks

None.