3.8.19.14 SEFC_SectorErase Function

C

bool SEFC_SectorErase( uint32_t address) 

Summary

Erases a Sector in the FLASH.

Description

This function determines the flash panel for the given address by calling `SEFC_FlashPanelGet` and then erases the corresponding sector (collection of pages).

Precondition

Validate if SEFCx controller is ready to accept new request by calling SEFC_IsBusy()

Parameters

ParamDescription
addressFLASH address to be Erased

Returns

Always returns true.

Example

SEFC_SectorErase(0x500000);

while(SEFC_IsBusy());

Remarks

Application needs to poll for busy bit or wait for callback to be called before sending next request.