2.77.4 OTPC_ReadPacket Function
C
otpc_error_code_t OTPC_ReadPacket( uint16_t headerAddress,
uint32_t *readBuffer,
uint16_t bufferSize,
uint16_t *sizeRead);
Summary
Reads a User packet from OTPC from a given address.
Description
Reads a packet from a given packet header address.
Precondition
OTPC_Initialize() function must have been called first and a valid packet should exist at the address.
Parameters
| Param | Description |
|---|---|
| headerAddress | Address of the packet |
| readBuffer | Pointer to the read buffer address |
| bufferSize | Size of the read buffer |
| sizeRead | Number of bytes read (output) |
Returns
OTPC error code
Example
OTPC_Initialize(); OTPC_ReadPacket(&packet, &payload, &headerAddress, &sizeWritten);
Remarks
None