2.12 Input Capture and Compare Timer
The Input Capture and Compare Timers block contains a 32-bit timer running at the main system clock frequency. The timer is free-running and is associated with six 32-bit capture registers and two compare registers. Each capture register can record the value of the free-running timer based on a programmable edge of its associated input pin. An interrupt can be generated for each capture register each time it acquires a new timer value. The timer can also generate an interrupt when it automatically resets and can additionally generate two more interrupts when the timer matches the value in either of two 32-bit compare registers.
Using the Library
volatile uint32_t capTimerCnt = 0;
volatile uint32_t diffCnt = 0;
volatile bool capInterrupt = false;
uint32_t freq = 0;
void cct_capture_callback(uintptr_t context)
{
uint32_t timerCnt = CCT_FreeRunningTimerGet();
if (timerCnt > capTimerCnt)
{
diffCnt = timerCnt - capTimerCnt;
}
else
{
diffCnt = (0xFFFFFFFF - capTimerCnt) + timerCnt;
}
capTimerCnt = timerCnt;
capInterrupt = true;
}
int main ( void )
{
/* Initialize all modules */
SYS_Initialize ( NULL );
printf("\n\r---------------------------------------------------------");
printf("\n\r CCT Capture Demo ");
printf("\n\r---------------------------------------------------------\n\r");
CCT_Capture0CallbackRegister(cct_capture_callback, 0);
CCT_FreeRunningTimerStart();
PWM0_Start();
while ( true )
{
if (capInterrupt == true)
{
freq = CCT_FrequencyGet()/diffCnt;
printf("Frequency : %ld Hz\r\n", freq);
capInterrupt = false;
}
}
/* Execution should not come here during normal operation */
return ( EXIT_FAILURE );
}Library Interface
Input Capture and Compare Timer peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| CCT_Initialize | Initializes given instance of CCT peripheral. |
| CCT_CaptureChannelxGet | Returns the free running timer counter value at the time of the channel's capture edge event occurred |
| CCT_CapturexCallbackRegister | Allows application to register a callback with for the CCT capture channel |
| CCT_CompareChannelxDisable | Disables compare channel |
| CCT_CompareChannelxEnable | Enables compare channel |
| CCT_CompareChannelxInterruptDisable | Disables compare channel interrupt |
| CCT_CompareChannelxInterruptEnable | Enables compare channel interrupt |
| CCT_CompareChannelxOutputClear | Sets the compare channel output low state |
| CCT_CompareChannelxOutputSet | Sets the compare channel output high state |
| CCT_CompareChannelxPeriodGet | Returns the compare period value |
| CCT_CompareChannelxPeriodSet | Sets the compare period value |
| CCT_ComparexCallbackRegister | Allows application to register a callback with for the CCT compare channel |
| CCT_CounterOverflowCallbackRegister | Allows application to register a callback with the PLIB |
| CCT_FreeRunningTimerGet | Returns the current value of the free running timer counter |
| CCT_FreeRunningTimerReset | Stops the free running timer and resets the internal counter to 0 |
| CCT_FreeRunningTimerSet | Sets the value of the free running timer counter |
| CCT_FreeRunningTimerStart | Starts the free running timer |
| CCT_FreeRunningTimerStop | Stops the free running timer |
| CCT_FreqDivSet | Sets the divisor value for the free running timer source clock |
| CCT_FrequencyGet | Returns the frequency of the clock source of free running timer |
| CCT_TimerActivate | Activates the CCT timer block |
| CCT_TimerDeActivate | De-activates the CCT timer block |
Data types and constants
| Name | Type | Description |
|---|---|---|
| CCT_CALLBACK | Typedef | Defines the data type and function signature for the CCT peripheral callback function. |