2.109 Single-Edge Nibble Transmission (SENT)
This Plib implements software abstraction for SENT Peripheral.
Library Interface
Single-Edge Nibble Transmission peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| SENTx_Initialize | Initializes the SENTx peripheral of the device |
| SENTx_Deinitialize | De-initializes the SENTx peripheral of the device |
| SENTx_Enable | Enables the SENTx peripheral of the device |
| SENTx_Disable | Disables the SENTx peripheral of the device |
| SENTx_Transmit | Transmits the data to the receiver when SENTx peripheral acts as a transmitter |
| SENTx_TransmitModeSet | Sets the SENTx peripheral transmit mode |
| SENTx_IsTransmissionComplete | Returns the transmit complete status |
| SENTx_TransmitStatusGet | Gets the transmission status of the SENTx peripheral module |
| SENTx_TransmitCompleteCallbackRegister | Registers a callback function to be called upon completing transmission for the SENTx peripheral |
| SENTx_Receive | Reads the received data at the receiver |
| SENTx_IsDataReceived | Checks if data has been received for SENTx peripheral |
| SENTx_ReceiveStatusGet | Retrieves the receive status SENTx peripheral |
| SENTx_ReceiveErrorGet | Returns the type of reception error |
| SENTx_ReceiveCompleteCallbackRegister | Registers a callback function to be called upon the completion of data reception for the SENTx peripheral |
| SENTx_ErrorCallbackRegister | Registers a callback function to be called upon encountering an error during data reception for the SENTx peripheral |
Data types and constants
| Name | Type | Description |
|---|---|---|
| SENT_DATA_RECEIVE | Struct | Configures the SENTx data receive packet |
| SENT_RECEIVE_STATUS | Enum | Defines the SENTx receive status |
| SENT_DATA_TRANSMIT | Struct | Configure the SENTx data transmit packet |
| SENT_TRANSMIT_MODE | Enum | Defines the SENTx transmission mode (Asynchronous and Synchronous) |
| SENT_TRANSMIT_STATUS | Enum | Defines the SENTx transmit status |
| SENT_ERROR_CODE | Enum | Defines the SENTx error code |
| SENT_ERROR_CALLBACK | Typedef | Defines a function pointer type for a callback function when error occurs |
| SENT_RECEIVE_COMPLETE_CALLBACK | Typedef | Defines a function pointer type for a callback function when data reception is complete |
| SENT_TRANSMIT_COMPLETE_CALLBACK | Typedef | Defines a function pointer type for a callback function when data is successfully transmitted |
Note: Not all APIs maybe implemented. See the specific device
family section for available APIs.