2.3 Analog Digital Converter (ADC)
This Plib implements software abstraction for ADC Peripheral.
Library Interface
Analog Digital Converter peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| ADCx_Initialize | Initializes ADC peripheral |
| ADCx_Enable | Enable (turn ON) ADC module |
| ADCx_Disable | Disable ADC module |
| ADC_SamplingStart | Starts the sampling |
| ADCx_ChannelSelect | Selects ADC input channel |
| ADCx_ConversionStart | Starts the ADC conversion of all the enabled channels with the software trigger |
| ADCx_ConversionStatusGet | Returns the status of the conversion of the channel |
| ADCx_ConversionResultGet | Returns the conversion result of the channel |
| ADCx_LastConversionResultGet | Returns the result for the previous adc conversion of the channel |
| ADCx_ConversionSequenceIsFinished | Returns the status of automatic sequence conversion |
| ADCx_ComparisonWindowSet | Returns the status of automatic sequence conversion |
| ADCx_WindowMonitorStatusGet | Returns the status of the window monitor flag |
| ADCx_ComparisonWindowSet | Returns the status of automatic sequence conversion |
| ADCx_WindowModeSet | This function configures the window comparison mode |
| ADCx_InterruptsClear | This function clears the interrupt flags |
| ADCx_InterruptsEnable | This function enables the interrupts |
| ADCx_InterruptsDisable | This function disables the interrupts |
| ADCx_CallbackRegister | Registers the function to be called from interrupt |
| ADCx_SoftwareTriggerEnable | Sets software common trigger |
| ADCx_ChannelSoftwareTriggerEnable | Sets individual software trigger |
| ADCx_ChannelResultGet | Returns the conversion value for the channel selected |
| ADCx_ChannelResultIsReady | Returns the status of conversion and determine if conversion is completed |
| ADCx_ChannelResultInterruptEnable | Enables individual channel interrupt |
| ADCx_ChannelResultInterruptDisable | Disables individual channel interrupt |
| ADCx_ChannelResultFlagClear | Clears individual channel interrupt flag |
| ADCx_CompareStatusGet | Returns the status of the comparator |
| ADCx_IndividualChannelInterruptPrioritySet | Allows selection of priority for individual channel interrupt |
| ADCx_ChannelCallbackRegister | Define custom callback for ADCx Channel event |
| ADCx_ComparatorCallbackRegister | Define custom callback for ADCx Comparator event |
| ADCx_PWMTriggerSourceSet | Sets Trigger source as PWM Trigger |
| ADC_InputSelect | Selects input for ADC |
| ADC_InputScanSelect | Selects input for scanning ADC channels |
| ADC_ResultIsReady | Returns the status of the channel conversion |
| ADC_ResultGet | Provides the ADC conversion result based on the buffer index |
| ADC_CompareEnable | Enables digital comparisons for the given channel on the specified ADC core |
| ADC_CompareDisable | Disables digital comparisons for the given channel on the specified ADC core |
| ADC_CompareWinThresholdSet | Configures the low and high threshold values for the comparator on the specified ADC core |
| ADC_CompareWinModeSet | Configures the low and high threshold values for the comparator on the specified ADC core |
| ADC_GlobalInterruptsStatusGet | Returns the global interrupt status |
| ADC_CoreInterruptsEnable | Enables the specified ADC core's interrupt |
| ADC_CoreInterruptsDisable | Disable the specified ADC core's interrupts |
| ADC_CoreInterruptsStatusGet | Returns the specified ADC core's interrupt status |
| ADC_CoreInterruptsStatusClear | Clears the specified ADC core's interrupt status |
| ADC_GlobalEdgeConversionStart | Generates global edge trigger and starts conversion on channels configured with Global edge as the trigger source |
| ADC_GlobalLevelConversionStart | Starts global level trigger and starts conversion on channels configured with Global level as the trigger source |
| ADC_GlobalLevelConversionStop | Stops global level trigger and stops conversion on channels configured with Global level as the trigger source |
| ADC_SyncTriggerEnable | Enables sync trigger defined by CTRLC.CNT value |
| ADC_SyncTriggerDisable | Disables sync trigger |
| ADC_SyncTriggerCounterSet | Configures the value of CTRLC.CNT register |
| ADC_SoftwareControlledConversionEnable | Enables software controlled conversion on the specified ADC core's channel |
| ADC_ChannelsEnable | Enables the ADC channels |
| ADC_ChannelsDisable | Disables the ADC channels |
| ADC_ChannelsInterruptEnable | Enables the ADC interrupt sources |
| ADC_ChannelsInterruptDisable | Disables the ADC interrupt sources |
| ADC_InterruptEnable | This function enables the interrupts |
| ADC_InterruptDisable | This function disables the interrupts |
| ADC_InterruptStatusGet | Returns the status of ADC interrupt |
| ADC_ChannelSamplingStart | Enables the Analog Mux Input and starts sampling on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelSamplingStop | Stops sampling on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelConversionStart | Starts conversion on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelResultIsReady | Returns the status of the channel conversion |
| ADC_ChannelResultGet | Reads the conversion result of the channel |
| ADC_EOSStatusGet | Indicates whether End of scan interrupt flag is set on the specified ADC core |
| ADC_ResultGet | Returns the ADC conversion value for the specified ADC core channel |
| ADC_FIFORead | Returns a single ADC conversion value from the ADC FIFO |
| ADC_FIFOBufferRead | Returns multiple ADC conversion values from the ADC FIFO |
| ADC_GlobalCallbackRegister | Registers the global callback function |
| ADC_COREnCallbackRegister | Registers the ADC core specific callback function |
| ADC_ConversionSequenceSet | Sets the user sequence of the channel conversion |
| ADCx_ComparisonWindowSet | Sets Low threshold and High threshold in comparison window |
| ADC_ComparisonEventResultIsReady | Returns the status of the Comparison event |
| ADC_ComparisonRestart | Restart the comparison function |
| ADC_SleepModeEnable | This function enables ADC sleep mode |
| ADC_SleepModeDisable | This function disables ADC sleep mode |
| ADC_FastWakeupEnable | This function enables ADC Fast Wakeup |
| ADC_FastWakeupDisable | This function disables ADC Fast Wakeup |
Data types and constants
| Name | Type | Description |
|---|---|---|
| ADC_MUX | Enum | Identifies which ADC Mux is to be configured |
| ADC_RESULT_BUFFER | Enum | Identifies which ADC buffer has to be read |
| ADC_INPUT_POSITIVE | Enum | Identifies possible positive input for ADC |
| ADC_INPUT_NEGATIVE | Enum | Identifies possible negative input for ADC |
| ADC_INPUTS_SCAN | Enum | Identifies possible ADC inputs which can be scanned |
| ADC_STATUS | Enum | Identifies ADC interrupt flag status |
| ADC_POSINPUT | Enum | Identifies ADC positive input pin to select |
| ADC_NEGINPUT | Enum | Identifies ADC negative input pin to select |
| ADC_WINMODE | Enum | Identifies ADC window comparison modes |
| ADC_CALLBACK | Typedef | Defines the data type and function signature for the ADC peripheral callback function |
| ADC_CALLBACK_OBJECT | Struct | ADC Callback structure |
| ADC_CORE_INT_CMPHIT | Macro | Identifies ADC core interrupt status |
| ADC_FIFO_CORID_GET | Macro | Returns the ADC core id in the ADC FIFO data |
| ADC_FIFO_DATA_GET | Macro | Returns the ADC conversion resunt from the ADC FIFO data |
| ADC_FIFO_CHNID_GET | Macro | Returns the ADC channel id in the ADC FIFO data |
| ADC_FIFO_CNT_GET | Macro | Returns the current number of entries present in the ADC FIFO |
| ADC_GLOBAL_INT_CRRDY1 | Macro | Identifies ADC global interrupt status |
| ADC_CHANNEL_MASK | Enum | Identifies ADC channel mask |
| ADC_CHANNEL_NUM | Enum | Identifies ADC channel number |
| ADC_INTERRUPT_EOC_MASK | Enum | Identifies EOC interrupt sources number |
| ADC_INTERRUPT_MASK | Enum | Identifies interrupt sources number |
| ADC_CORE_NUM | Enum | Identifies ADC core |
| ADC_CORE_CALLBACK | Typedef | Defines the function pointer data type and function signature for the adc peripheral core callback function |
| ADC_GLOBAL_CALLBACK | Typedef | Defines the function pointer data type and function signature for the adc peripheral global callback function |
| ADC_CORE_CALLBACK_OBJECT | Struct | ADC Core events Callback structure |
| ADC_GLOBAL_CALLBACK_OBJECT | Struct | ADC Global Callback structure |
| ADCx_CHANNEL | Enum |
Defines the ADC channels that are selected |
| ADCx_PWM_INSTANCE | Enum | Defines the ADC PWM trigger sources that are available for the module to use |
| INTERRUPT_PRIORITY | Enum |
Defines the interrupt priority values |
| ADC_CHANNEL_CALLBACK | Typedef | Callback function prototype for ADC Channel conversion complete interrupt |
| ADC_CMP_CALLBACK | Typedef | Callback function prototype for ADC Comparator event |
| ADC_PWM_TRIGGERS | Enum | Defines the PWM triggers that are available in each individual PWM |
Note: Not all APIs maybe implemented. See the specific device family
section for available APIs.