2.85.6 PMP_PortIsBusy Function
C
bool PMP_PortIsBusy( void )
Summary
Identifies if the (Master mode) PMP port is busy.
Description
This function identifies if the PMP port is busy (in Master mode).
Precondition
PMP should have been initialized by calling PMP_Initialize and configured for Master mode.
Parameters
None.
Returns
- true - If the port is busy
- false - If the port is not busy
Example
bool status; PMP_Initialize(); PMP_AddressSet(0x1); status = PLIB_PMP_PortIsBusy( PMP_ID_0 );
Remarks
None.