2.6.3 AIC_INT_IrqDisable Function
C
bool AIC_INT_IrqDisable ( void )
Summary
Disable interrupt to the processor.
Description
AIC will not generate interrupts to the processor when an interrupt condition is met.
Precondition
AIC should be initialized with a call to AIC_Initialize() function.
Parameters
None.
Returns
Current interrupt state.
Example
bool state = AIC_INT_IrqDisable ( );
Remarks
None.