2.30.6 DIVAS_SquareRoot Function
C
uint32_t DIVAS_SquareRoot(uint32_t number)
Summary
This function uses the DIVAS peripheral to perform a square root operation.
Description
This function uses the DIVAS peripheral to perform a square root operation. The function will return the square root of the 32-bit unsigned input number.
Precondition
The peripheral should have been initialized by calling the DIVAS_Initialize() function once.
Parameters
| Param | Description |
|---|---|
| number | unsigned number whose square root needs to be obtained |
Returns
The function returns the square root of the value contained in the number parameter.
Example
int32_t number;
uint32_t squareroot;
number = 144;
squareroot = DIVAS_SquareRoot(number);
Remarks
None.