2.40.2 EEPROM_WordRead Function
C
bool EEPROM_WordRead( uint32_t addr, uint32_t *data )
Summary
Reads one word from a given address in data EEPROM
Description
Reads one word from a given address in data EEPROM into the user buffer
Precondition
None
Parameters
| Param | Description |
|---|---|
| addr | Address of data EEPROM to be read from |
| data | pointer to user data buffer |
Returns
Returns true on success false on error
Example
uint32_t i; unint32_t readData[4]; uint32_t addr = 0; for ( i = 0; i < 4; i++ ) { result = EEPROM_WordRead( addr, &readData[i] ); if (result == true) { addr = eepromAddr + 4; } }