4.3 Data and Result Area

The data and result area is used to list and visualize the received measurement data. The decoded information from the byte-stream is shown in the data table and includes the following data:
  • Data Set – Measurement number
  • Distance – Distance between Verifier and Prover in cm
  • Offset – Measured clock offset between Verifier and Prover in ppm
  • Error Counter – Number of lost UWB measurements
During an active distance measurement, the data table is filled from top to bottom and scrolls down automatically. To deactivate the auto-scroll function, deselect “AutoScroll”.
Figure 4-7. Distance vs Frequency of Occurrence Diagram
Before starting a measurement, select the desired diagram type to visualize the result.
  • Under “Diagram Type”, select “Distance/Num” to display the measurement result as a bar diagram.
  • Under “Diagram Type”, select “Distance/Time” to display the measurement result (distance over time) as a line diagram.
Figure 4-8. Distance Over Time Diagram
Note: If it is necessary to delete all the received measurement results without interrupting a running measurement, click Clear View. This removes the content from the data table and the diagram chart too.