28.4 __builtin_bswap16 Built-in Function
Returns its argument with the order of its bytes reversed. For example, an argument value of 0xaabb is returned as 0xbbaa. A byte here always means exactly 8 bits.
Prototype
uint16_t __builtin_bswap16 (uint16_t x)
Argument
x: the value whose bytes are to be swapped
Return Value
The byte-swapped value
Error Messages
None.