28.20 __builtin_section_begin Built-in Function
Remember: This built-in
function gets run-time information about section addresses and sizes.
Description
Return the beginning address of the quoted section name.
Prototype
unsigned long __builtin_section_begin(quoted-section-name);
Argument
quoted-section-name The name of the section.
Return Value
The address of the section.
Assembler Operator/ Machine Instruction
.startof.
Error Messages
An “undefined reference” error message will be displayed if the quoted section name does not exist in the link.