15.2.1 Access Function Attribute
The access(access-mode, ref-index[,
size-index]) attribute provides
additional information about how a function accesses memory. It can assist
in diagnosing potential bugs related to memory access via compiler warnings
and help the compiler perform better optimizations.
The ref_index argument is the index (starting
from the left with index 1) of the function pointer argument that points to
the target object being accessed. A function pointer argument can be
referenced by at most one distinct access attribute.
access_mode argument specifies the type of
memory access made by the pointer referenced by the
ref_index and can be one
of:read_only- The pointer only reads from the target object. Unless
the indexed size argument is zero, the target object
must be initialized. This check is more robust than
just using the
constqualifier with the target as it cannot be cast away. write_only- The pointer (which cannot be to a
const-qualified type) only writes to the target object. The object referenced by the pointer need not be initialized. read_write- The pointer (which cannot be to a
const-qualified type) both reads from and writes to the target object. Unless the indexed size argument is zero, the target object must be initialized. none- The pointer does not access the target object at all.
Unless the pointer is
NULL, the target object must exist and have at least the size held by the size-index argument. If the size-index argument is omitted for a pointer ofvoid *type, the actual pointer argument is ignored. The referenced object need not be initialized. The mode is intended to be used as a means to help validate the expected object size, for example in functions that call__builtin_object_size.
The optional size_index argument is the index
of the function argument that specifies the number of elements of the
pointer type referenced by ref-index, or
the number of bytes when the pointer type is void *. When
this argument is not specified, the pointer argument must be either
NULL or point to a space that is suitably aligned
and sized for at least one object of the referenced type (this implies that
a past-the-end pointer is not a valid argument). The actual size of the
access may be less but it must not be more.
access attribute to
declare that the pointer argument to puts() will only read
its target of unspecified size. The attribute is used again to indicate that
the second argument to memcpy() only reads its target and
that this target has a size indicated by the value of the third function
argument.__attribute__ ((access (read_only, 1))) int puts(const char *);
__attribute__ ((access (read_only, 2, 3))) void * memcpy(void *, const void *, size_t);