15.2.35 Used Function Attribute
The
used attribute indicates to the compiler that the function
is always used and code must be generated for the function even if the
compiler cannot see a reference to the function. Such might be the case if
inline assembly is the only reference to a static function.
For
example:void __attribute__ ((used)) foo(void);