2.2 Design Checklist

The following table lists the various checks that design engineers must take care while designing a system.

Table 2-1. Design Checklist
GuidelineYes/NoRemarks
Prerequisites
– See PolarFire SoC Datasheet.

– See PolarFire SoC FPGA Packaging and Pin Descriptions User Guide.

——
Refer to the board-level schematics of PolarFire SoC Evaluation Kit——
Device Selection
Check for available device variants for PolarFire SoC FPGA

– Select a device based on I/O pin count, transceivers, package, phase-locked loops (PLLs), and speed grade

——
Check device errata in PolarFire SoC FPGA Errata (yet to be published)——
Design Checklist
Power Analysis

Download the PolarFire and PolarFire SoC FPGA Power Estimator and check for the power budget.

For more information, see UG0897: PolarFire and PolarFire SoC FPGA Power Estimator User Guide.

——
Power Supply Checklist

See Power Supplies for used power rails. See Unused Power Supply and Figure   2 for unused rails.

——
Decoupling Capacitors

Follow PolarFire SoC Decoupling Capacitors. Perform PI Analysis for any deviation from the recommended capacitors.

——
Clocks
For more information about dynamic phase shift ports, see Table 6 of PolarFire FPGA and PolarFire SoC FPGA Clocking Resources User Guide.

The XCVR reference clock ranges from 20 MHz to 400 MHz.

——
The global clock network can be driven by any of the following:

– Preferred clock inputs (CLKIN_z_w)

– On-chip oscillators

– CCC (PLL/DLL)

– XCVR interface clocks

High-Speed I/O Clocks

High-speed I/O clock networks can be driven by I/O or CCCs. The 
high-speed I/O clocks can feed reference clock inputs of adjacent CCCs through hardwired connections.

CCC

The CCC can be configured to have a PLL or DLL clock output, driving a high-speed I/O clock network.

——
Global buffer (GB) can be driven through the dedicated global I/O, CCC or fabric (regular I/O) routing. The global network is composed of GBs to distribute low-skew clock signals or high-fanout nets.

Dedicated global I/O drive the GBs directly and are the primary source for connecting external clock inputs (to minimize the delay) to the internal global clock network.

For more information about global clock network, see PolarFire FPGA and PolarFire SoC FPGA Clocking Resources User Guide.

——
Reset
For more information about DEVRST_N and user reset, see Reset.——
DDR Interface
For more information about DDR routing and topology, see PolarFire FPGA and PolarFire SoC FPGA Memory Controller User Guide.——
Programming and Debugging Scheme

For programming and debugging information, see Device Programming.

——
XCVR
For more information about XCVR, see PolarFire FPGA and PolarFire SoC FPGA Transceiver User Guide.——
For I/O gearing interfaces, place the clocks and data based on the defined requirements by selecting the correct I/O. For more information about the placement of User I/O, see PolarFire FPGA and PolarFire SoC FPGA User I/O User Guide.——
There is one IO_CFG_INTF pin available, which can be used as input.——
See the bank location diagrams in the

PolarFire SoC FPGA Packaging and Pin Descriptions User Guide to assess the preliminary placement of major components on PCB.

——