4 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

RevisionDateDescription
F08/2024The following is a summary of changes made in this revision.
  • Following changes have been made in Table 1-8:
    • Updated the decoupling capacitor part number for 2.2 nF.
    • Added the decoupling capacitor part numbers for 1 µF and 47 nF.
  • Added a note under Table 1-1 to clarify the VDDI5 power-up sequence.
  • Removed instances of SPI_EN and IO_CFG_INTF pins from Figure 1-6 in JTAG Programming section as they are not used during JTAG programming.
  • Updated Brownout Detection for a note related to the brownout detection on any PolarFire supply.
E11/2023The following is a summary of changes made in this revision.
  • Updated Figure   1 and Figure   2 by changing the power supply name from “VDDIO (MSS SGMII Bank 5)” to “VDDI5”.
  • Revised information regarding the VDDI5 power supply. See Table   1.
  • Changed the number of 47 µF decoupling capacitors to be used for VDDA25 in Table 1-5.
  • Updated Figure 1-2 by changing the power supply name from “VDDI Bank 5 (MSS SGMII)” to “VDDI5”.
  • Revised a note about GPIO glitch during JTAG programming. See I/O Glitch.
  • Substituted Figure 1-5 with a high-quality image.
D10/2023The following is a summary of changes made in this revision.
  • Updated Power Supplies as follows:
    • Added information about target impedance.
    • Updated Figure 1-1 by adding operating voltage 1.1V to VDDIO (MSS DDR Bank 6).
    • Added a note describing that the 1.1V operating voltage for VDDIO (MSS DDR Bank 6) is for the LPDDR4 support. Also, added a link to PolarFire Family Memory Controller User Guide.
  • Updated PolarFire SoC Decoupling Capacitors as follows:
    • Added power supply decoupling capacitor details for MPFS460TS - FCG1152 and MPFS095TS/MPFS025TS - FCS325 devices.
    • Updated the power supply decoupling capacitor details for MPFS250TS/MPFS160TS/MPFS095TS - FCG1152, FCSG536, FCVG484, and FCVG784 devices.
  • Added a note about GPIO glitch during JTAG programming. See I/O Glitch.
  • Replaced “VDDSREF” with “VDD_XCVR_CLK” throughout all the decoupling capacitors tables in PolarFire SoC Decoupling Capacitors.
  • Added Table 1-5 and Table 1-6.
  • Updated the unused condition of VDDI Bank 5 (MSS SGMII) to 2.5/3.3V in Figure 1-2.
C05/2022The following is a summary of changes made in this revision.
  • In Power Supplies, added a note about power sequencing requirement for I/O calibration.
  • Updated I/O Glitch.
  • Updated Clocks to highlight regional clock implications while migrating designs to different device sizes.
  • Updated Figure 1-9.
  • Added a note about hot socketing exceptions in Hot Socketing (GPIO Only).
  • Added link to PPAT in Clocks for preferred clock inputs connectivity to PLLs, DLLs, and global clock network.
  • Enabled ‘Ask A Question’ hyperlink for each section in the document.
B10/2021The following is a summary of changes made in this revision.
  • Updated Table 1-9 for power-up and power-down sequencing requirements for mitigating I/O glitch.
  • Added recommended 1 nF, 2.2 nF, 10 nF, and 0.1 µF decoupling capacitors of the 0402 size for the 1 mm package. See Table   7.
  • Added more information in new footnotes for VDD and VDDA in Table   1.
  • Added footnotes for all decoupling capacitor tables in PolarFire SoC Decoupling Capacitors to specify the objective of decoupling capacitors.
A01/2021The following is a summary of changes made in this revision.
1.0—The first publication of this document.