1.1.2 Unused Power Supply
(Ask a Question)The following figure shows how power supplies can be configured when not in use and when you need to reduce leakage and power for the system.
The following figure shows the power configuration of unused supplies. This option can be used when there is an intent to power-up the various supplies at a later time in the system, and the I/Os are not being used.
Important: To simplify the board-level routing, multiple 10 kΩ
resistors can be used as required. The power supplies can also be grouped into a single 10
kΩ resistor and tied-off to VSS.