8.1 Byte Write
A byte write requires the following sequence and is depicted in Figure 8-1. After the CS line is
pulled low to select the device, the WRITE (02h) instruction is
transmitted via the SI line, followed by the 16‑bit address and the data (D7‑D0) to be
programmed. Programming will start after the CS pin is brought
high. The low‑to‑high transition of the CS pin must occur during
the SCK low time (Mode 0) and SCK high time (Mode 3) immediately after clocking in the D0
(LSB) data bit. The AT25128B/AT25256B is automatically returned to
the Write Disable state (STATUS register bit WEL = 0) at the completion of
a write cycle.
- This instruction initiates a self-timed internal write cycle (tWC) on the rising edge of CS after a valid sequence.