8 Write Sequence
In order to program the AT25128B/AT25256B, two separate instructions
must be executed. First, the device must be write enabled via the Write Enable
(
WREN) instruction. Then, one of the two possible write sequences
described in this section may be executed. Note: If the device is not Write Enabled
(
WREN), it will ignore the WRITE instruction
and will return to the Standby state when CS is brought
high. A new CS assertion is required to re-initiate
communication.The address of the memory location(s) to be programmed must be outside the protected
address field location selected by the block write protection level. During an internal
write cycle, all commands will be ignored except the
RDSR instruction.
Refer to Table 8-1 for the AT25128B/AT25256B address bits.| Address | AT25128B | AT25256B |
|---|---|---|
| AN | A13–A0 | A14–A0 |
| Don’t Care Bits | A15–A14 | A15 |