8.2 Page Write
A page write sequence allows up to 64 bytes to be written in the same
write cycle, provided that all bytes are in the same row of the memory array. Partial page
writes of fewer than 64 bytes are allowed. After each byte of data is received, the six
lowest-order address bits are internally incremented following the receipt of each data
byte. The higher-order address bits are not incremented and retain the memory array page
location. If more bytes of data are transmitted than what will fit at the end of that
memory row, the address counter will roll over to the beginning of the same row.
Nevertheless, creating a rollover event should be avoided, as previously loaded data in the
page could become unintentionally altered. The AT25128B/AT25256B
is automatically returned to the Write Disable state (WEL = 0) at the
completion of a write cycle.
- This instruction initiates a self‑timed internal write cycle (tWC) on the rising edge of CS after a valid sequence.