4.9.16 Equ Directive
EQU
pseudo-op defines a symbol and equates its value
to an expression. For example:thomas EQU 123h
The identifier thomas
will be given the value 123h.
EQU
is legal only when the symbol has not previously been defined. See
Set Directive for
redefinition of values.
This directive does not reserve memory for the symbol specified.
Use the DS
directive to reserve data memory (see Ds Directive). An
EQU
performs a similar function to the preprocessor’s
#define
directive (see Preprocessor Directives).
Since EQU
directives do not contribute to the output, they are processed
separately to other instructions and directives. Thus, the program location counter cannot
be used in EQU
operand expressions.