3.4.37 X: Specify Source Language Option
The -xlanguage option allows you to specify that
the source files that follow are written in the specified language, regardless of the
extension they use.
The languages allowed by the assembler are tabulated below.
| Language | Description |
|---|---|
assembler | Assembly source code |
assembler-with-cpp | Assembly source code that must be preprocessed |
For example, the command:
pic-as -mcpu=18f4520 -c -xassembler-with-cpp init.swill tell the assembler to run the preprocessor
over the assembly source file, even though the init.s file name does not
use a .S extension.