3.4.28 Save-temps Option
The -save-temps option instructs the assembler to keep
temporary files after compilation has finished.
The intermediate files will be placed in the current directory and have a
name based on the corresponding source file. Thus, compiling foo.s
with -save-temps would produce the foo.o object
file.
The -save-temps=cwd option is equivalent to
-save-temps.
The -save-temps=obj form of this option is similar to
-save-temps, but if the -o option is specified, the
temporary files are placed in the same directory as the output object file. If the
-o option is not specified, the -save-temps=obj switch
behaves like –save-temps.