2.2 Design Steps

  1. Select R2: The lower feedback resistor R2 is selected in the kΩ range to limit the feedback divider bias current.

    For this design example, R2 = 3 kΩ is selected, considering VREF = 0.6V and approximately 200 μA bias current.

  2. Calculate R1: Once R2 is selected, R1 is calculated based on the required output voltage using:
    Equation 2-1. 
    R 1 = R 2 V OUT V REF - 1

    For VOUT = 5V, the calculated value is: R1 = 22 kΩ

  3. Choose FC: The crossover frequency is selected between FSW/10 and FSW/20. Since FSW = 266 kHz, a crossover frequency of FC = 20 kHz is chosen.
  4. Calculate ΔVFB: The feedback ripple must be within 40 mV to 200 mV, unless otherwise specified in the data sheet. It is estimated using:
    Equation 2-2. 
    V FB = V O · ( 1 - D ) 2 π · L · C OUT · F C · F SW

    For this design, the initial calculated feedback ripple is: ΔVFB = 130 mV. This value must be recalculated after selecting CFF and RINJ.

  5. Calculate CFF: The feed-forward capacitor is selected to place the second zero slightly below FC.

    In this example, FZ2 is placed at F C / 3 , providing sufficient phase boost at crossover. So, CFF can be calculated using:

    Equation 2-3. 
    C FF = 3 2 π · R 1 · F C

    The calculated value is approximately: CFF = 630 pF. For testing, the value selected is: CFF = 560 pF.

  6. Calculate RINJ: The ripple injection resistor is calculated using rearranged Equation 1-20 as:
    Equation 2-4. 
    R INJ = V O ( 1 - D ) ΔV FB C FF F SW

    The calculated value is approximately: RINJ = 230 kΩ. For practical implementation and testing, the standard value selected in this example is: RINJ = 200 kΩ.

  7. Recalculate Feedback Ripple (ΔVFB): After selecting practical component values for CFF and RINJ, it is important to recalculate the resulting feedback ripple to account for deviations from the ideal calculated values.

    For CFF = 560 pF and RINJ = 200 kΩ, the recalculated feedback ripple is: ΔVFB = 150 mV.

    It is essential to verify that this final value lies within the recommended operating range specified for the device. Ensuring that the feedback ripple remains within this range is critical for maintaining proper comparator operation, avoiding noise sensitivity or jitter, and achieving stable and predictable control loop performance.

  8. Calculate FLC and CINJ: The LC resonant frequency is calculated first using Equation 1-20. For this design: FLC = 5 kHz. The DC blocking capacitor CINJ is then selected to place the first zero 1-2 decades below FLC.

    In this example, first zero is placed two decades below FLC. So CINJ can be calculated using:

    Equation 2-5. 
    C INJ = 10 2 2 π R INJ F LC

    The calculated value is: CINJ = 15.9 nF. For testing, the selected value is: CINJ = 15 nF.

  9. Verify Stability Criteria: The final step is to ensure we meet the required stability criteria. The impedance of CFF at the switching frequency should be much smaller than the equivalent feedback resistance (R1‖R2), so that the current through the feedback resistors can be neglected, allowing the feed-forward capacitor to effectively couple the switching ripple to the feedback node. This can be verified using:
    Equation 2-6. 
    1 2 π · C FF · F SW R 1 R 2

    For the selected values: 1.06 kΩ < 2.64 kΩ. This confirms that the stability criterion is satisfied. Therefore, the ACOT control loop design is complete. However, final validation must always be performed on the bench to confirm feedback ripple, phase margin, and transient response.