6.4 Streaming Variable Values
Select the source for streaming.
Set up the connection by clicking the gear icon. For DVRT, use the values shown in the figure below.
Note: For all implementations of DVRT, use the Baud Rate of
115200.
Click the Play button to start streaming. Once streaming has started, a toggle button will be made active where you can Stop Streaming/Start Streaming.
See the variable values change during runtime in the table.
If you want change value format, in this case view Int values in hex, you can use the controls on the right to select available options.