5 Response Time
The response time refers to the time between the physical touch of a button and a touch reported to the host.
Response times change with the following configurations:
- Measurement Period
- Frequency Hop
- CSD
- Measurement Clock Frequency
- Detect Integration (DI)
- Response Time
- Oversampling (Filter Level)
Refer to the following topics for more information.
Best-Case Response Time
The best-case response time is calculated when the button is touched before its measurement. The formula to calculate the best-case response time is present in the Formula chapter.
Worst-Case Response Time
The worst-case response time is calculated when the button is touched just after it was measured. The formula to calculate the worst-case response time is present in the Formula chapter.