3.9.1 Frequency Hop
Operation
The Frequency Hop feature varies the touch measurement frequency between consecutive measurements. Response time slightly increases with Frequency Hop enabled. A typical increase in response time would be one Measurement Period. Refer to the Response Time for more information.
The three frequencies to acquire touch are pre-defined by the host. Refer to the Hop Frequency (FREQ) register. The MTCH2120 user has complete control over the used frequencies. During run-time, the host can change these frequencies.
Initialization
The Frequency Hop feature is enabled by writing 1 to FREQHOP bit the
Device Control (DEVCTRL) register. The three frequencies must be defined in FREQ[n]
registers.
Enabling or disabling these features by the Host does not require a reset after the configuration update. Refer to the Configuration Summary for more details.
Steps to Configure Frequency Hop
- Different frequencies can be
selected by writing in the FREQ[n] register. Frequencies will be taken into
effect from the following measurement. Refer to the Hop Frequency for
details on the possible values and offset address.Note: The Autotune feature must be disabled before writing the register. See section 3.8.2.
- The Frequency Hop feature is
enabled by writing
1in DEVCTRL.FREQHOP register. - Save the Settings
(optional):Note: Use the "save" command to apply the updated configuration after resetting the device. Otherwise, this step is optional.
- Write
1in DEVCTRL.SAVE to save the configuration
- Write