17.7.3 Generator Control (GENCTRL0,2,3,4,5,6,7)

GENCTRLn controls the settings of Generic Generator n (n=0,2,3,4,5,6,7) (PIC32CM2532 and PIC32CM5164 devices).

GENCTRLn controls the settings of Generic Generator n (n=0,2,3,4) (PIC32CM1216 devices).

Important: GENCTRL1 has its own register described in GENCTRL1 register.

A User Reset will reset the associated GENCTRLn registers unless the Generator is the source of a locked Peripheral Channel m (PCHCTRLm.WRTLOCK=1).

Note: GENCTRLn is a write-synchronized register: SYNCBUSY.GENCTRLn must be checked to ensure the GENCTRLn synchronization is complete.
Name: GENCTRLn
Offset: 0x20,0x28,0x2C,0x30,0x34,0x38,0x3C
Reset: 0x00000105 (GENCTRL0), 0x00000000 (others)
Property: PAC Write-Protection, Write-Synchronized

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
 DIV[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 
Bit 15141312111098 
   RUNSTDBYDIVSELOEOOVIDCGENEN 
Access R/WR/WR/WR/WR/WR/W 
Reset 00000x 
Bit 76543210 
     SRC[3:0] 
Access R/WR/WR/WR/W 
Reset xxxx 

Bits 23:16 – DIV[7:0] Division Factor

These bits represent a division value for the corresponding Generator. The actual division factor is dependent on the state of DIVSEL.

Bit 13 – RUNSTDBY Run in Standby

This bit is used to keep the Generator running in Standby as long as it is configured to output to a dedicated GCLK_IO[n] pin. If GENCTRLn.OE is zero, this bit has no effect and the generator will only be running if a peripheral requires the clock.

ValueDescription
0The Generator is stopped in Standby and the GCLK_IO[n] pin state (one or zero) will be dependent on the setting in GENCTRL.OOV.
1The Generator is kept running and output to its dedicated GCLK_IO[n] pin during Standby mode.

Bit 12 – DIVSEL Divide Selection

This bit determines how the division factor of the clock source of the Generator will be calculated from DIV. If the clock source should not be divided, DIVSEL must be 0 and the GENCTRLn.DIV value must be either 0 or 1.

ValueDescription
0The Generator clock frequency equals the clock source frequency divided by GENCTRLn.DIV.
1The Generator clock frequency equals the clock source frequency divided by 2^(GENCTRLn.DIV + 1).

Bit 11 – OE Output Enable

This bit is used to output the Generator clock output to the corresponding pin (GCLK_IO[n]), as long as GCLK_IO[n] is not defined as the Generator source in the GENCTRLn.SRC bit field.

ValueDescription
0No Generator clock signal on pin GCLK_IO[n].
1The Generator clock signal is output on the corresponding GCLK_IO[n], unless GCLK_IO[n] is selected as a generator source in the GENCTRLn.SRC bit field.

Bit 10 – OOV Output Off Value

This bit is used to control the clock output value on pin (GCLK_IO[n]) when the Generator is turned off or the OE bit is zero, as long as GCLK_IO[n] is not defined as the Generator source in the GENCTRLn.SRC bit field.

ValueDescription
0The GCLK_IO[n] will be LOW when generator is turned off or when the OE bit is zero.
1The GCLK_IO[n] will be HIGH when generator is turned off or when the OE bit is zero.

Bit 9 – IDC Improve Duty Cycle

This bit is used to improve the duty cycle of the Generator output to 50/50 for odd division factors.

ValueDescription
0Generator output clock duty cycle is not balanced to 50/50 for odd division factors.
1Generator output clock duty cycle is 50/50.

Bit 8 – GENEN Generator Enable

This bit is used to enable and disable the Generator.

ValueDescription
0Generator is disabled.
1Generator is enabled.

Bits 3:0 – SRC[3:0] Generator Clock Source Selection

These bits select the Generator clock source, as shown in this table.

Table 17-4. Generator Clock Source Selection
ValueNameDescription
0x00XOSCXOSC oscillator output
0x01GCLK_INGenerator input pad (GCLK_IO[n])
0x02GCLK_GEN1Generic clock generator 1 output
0x03OSCULP32KOSCULP32K oscillator output
0x04XOSC32KXOSC32K oscillator output
0x05OSC16MOSC16M oscillator output
0x06DFLLULPDFLLULP ultra low power output
0x07DFLL48MDFLL48M output
0x08FDPLL96MFDPLL96M output
0x09-0x0FReservedReserved for future use