53.3 External Analog Reference Connections
The following schematic checklist is only necessary if the application is using one or more of the external analog references. If the internal references are used instead, the circuits in the following two figures are not necessary.
| Signal Name | Description | Recommended Pin Connection |
|---|---|---|
| VREFx | External reference VREFA/VREFB |
Capacitors(2): refer to REG_9(1) |
| AVSS | Ground | - |
Note:
- Refer to Power Supply Electrical Specifications from the “Electrical Characteristics” chapter.
- Decoupling capacitors must be placed close to the device, and low ESR capacitors must be used for better decoupling.