47.6.2 Crystal Oscillator
The crystal oscillator schematic is shown below:
The crystal must be located as close to the device as possible. Long-signal lines may cause too high of a load to operate the crystal, and cause crosstalk to other parts of the system.
| Signal Name | Recommended Pin Connection | Description |
|---|---|---|
| XIN | Load capacitor. Value depends on Crystal manufacturers recommendation.(1) | External crystal between 0.4 to 32 MHz |
| XOUT | Load capacitor. Value depends on Crystal manufacturers recommendation.(1) |
Note:
- The capacitors must be placed close to the device for each supply pin pair in the signal group.