3.3.2 Host Mode

In Host mode, plug the ATA8510 Curiosity Board into a host MCU using the mikroBUS™ header with the control interface.

In this configuration, the host board supplies power to the ATA8510 Curiosity Board, and a USB Type-C™ cable is not required. Refer to Table 3-2 for the jumper settings to use with the host board.

The ATA8510 Curiosity Board communicates with the host board over the SPI via the mikroBUS socket. Refer to the following table for the pinouts on the ATA8510 Curiosity Board mikroBUS interface.

CAUTION:
  • In Host mode, ensure that the USB Type-C cable is disconnected.
  • All ATA8510 Curiosity Boards have to be programmed with Atmel-ICE in Standalone mode before use for Host mode with a host board.
Figure 3-7. Interface with Host
Figure 3-8. mikroBUS™ Pinout Diagram
Table 3-4. mikroBUS™ Header Pin Description – J101, J102 (2)
Pin NumberPin on mikroBUS™ SocketPin Description of mikroBUS™ SocketPin on the ATA8510 RF Board(1)
J101-1ANAnalog inputPWRON/PCINT4/LED1/PB4
J101-2RSTResetNRESET/PCINT8/debugWIRE/PC0
J101-3CSSPI Chip Select (CS)PCINT5/INT1/NSS/PB5
J101-4SCKSPI clockPCINT1/SCK/PB1
J101-5MISOSPI Host Input Client OutputPCINT3/MISO/PB3
J101-6MOSISPI Host Input Client InputPCINT2/MOSI/PB2
J101-7+3.3V3.3V power NC
J101-8GNDGroundGND
J102-8GNDGroundGND
J102-7+5V5V power NC
J102-6SDAI2C dataNPWRON5/PCINT13/TRPB/TMDO_CLK/PC5
J102-5SCLI2C clockPCINT0/CLK_OUT/PB0
J102-4RXUART receiveNPWRON3/PCINT11/TMDO/TxD/PC3
J102-3TXUART transmitNPWRON4/PCINT12/INT0/TMDI/RxD/PC4
J102-2INTHardware interruptPCINT6/EVENT/PB6
J102-1PWMPWM outputNPWRON1/PCINT9/EXT_CLK/PC1
Note:
  1. For more details on the ATA8510 pins, refer to the ATA8510/15 Industrial Data Sheet (DS70005505).
  2. These are alternate function pins that can be configured for any of the supported peripheral functions based on the end user application.